MODBUS.WATCHDOG
Description
MODBUS.WATCHDOG is the watchdog timeout in seconds.
The Modbus watchdog fault, F7100, is generated if the drive does not receive any Modbus messages within a time window set by MODBUS.WATCHDOG. Zero disables the watchdog.
Context
For more information, see Handling Broken Connections.
Versions
Action | Version | Notes |
---|---|---|
Implemented |
02-05-00-000 |
General Information
Type |
Read Write Parameter |
Units |
Seconds |
Range |
0 to 60 |
Default Value |
5 |
Data Type |
Integer |
See Also |
Fault F7100 |
Stored in Non-Volatile Memory |
Yes |
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
---|---|---|---|---|---|---|---|
MODBUS.WATCHDOG |
3014h |
05h |
Unsigned16 |
- |
- |
Read/Write |
No |
Name |
ID |
Hex |
Data Type |
Access |
Units |
---|---|---|---|---|---|
MODBUS.WATCHDOG |
3709 |
E7D |
Unsigned16 |
Read/Write |
- |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
MODBUS.WATCHDOG |
3709 |
Unsigned16 |
Read/Write |
- |